The product described is a gas-actuated fastening tool. It is designed to drive suitable fasteners (nails) into concrete, steel, concrete-block masonry, sand-lime block, rendered masonry and other materials suitable for use of the direct fastening technique.
The fastening tool, gas can, battery and fasteners form a technical unit. This means that trouble-free fastening with this fastening tool can be ensured only when it is used together with the fasteners, gas cans and batteries specially manufactured for it by
Hilti . The fastening and application recommendations made by
Hilti apply only when these conditions are observed.
The fastening tool is for hand-held use only.
- Use only Hilti Li‑ion batteries of the B 12 series with this product.
- Use only Hilti battery chargers of the C 4/12-50 series for charging these batteries.
Gas-actuated fastening tool with fastener guide, 2 batteries, charger, toolbox and operating instructions.
Other system products approved for use with this product can be found at your local
Hilti Center or online at:
www.hilti.com
The fastener guide holds the studs or, respectively, guides the nails and, when the tool is actuated, thus directs the fasteners into the supporting material at the desired position.
The slider can be used to reduce the depth to which the fastener is driven. In the
EJECT position, it releases the fastener guide for removal.
Status
|
Meaning
|
+
|
Standard fastener driving depth
|
‑
|
Reduced fastener driving depth
|
EJECT
|
Fastener guide release
|
On an even working surface, the support leg makes it easier to hold the fastening tool perpendicular as attention then only has to be paid to lateral alignment. On an uneven or undulating surface it may be necessary to remove the support leg in order to allow the fastener guide to be held perpendicular to the working surface.
The belt hook can be extended in three stages.
Status
|
Meaning
|
Position 1
|
Position for attaching to a waist belt
|
Position 2
|
Position for attaching to ladders, scaffolds, platforms, etc.
|
Position 3
|
Belt hook removed
|
Observe the safety instructions provided with the gas can!
In order to operate the fastening tool, the gas can must be inserted in the gas can compartment.
The gas can status can be read from the LED display after pressing the
GAS button.
The gas can must be removed before breaks between working, before maintenance and before transporting or storing the fastening tool.
After pressing the
GAS button, the LED display indicates the status of the gas can.
Status
|
Meaning
|
All four LEDs light green.
|
The level is between 100 % and 75 %.
|
Three LEDs light green.
|
The level is between 75 % and 50 %.
|
Two LEDs light green.
|
The level is between 50 % and 25 %.
|
One LED lights green.
|
The level is between 25 % and 10 %.
|
One LED blinks green.
|
- Level is below 10 %. Replacement of the gas can is recommended.
- The gas can is empty or is malfunctioning. Replacement of the gas can is recommended.
Even when the level is indicated as “empty”, the gas can, for technical reasons, still contains a little gas.
|
One LED blinks red.
|
No gas can or the wrong type of gas can is present in the fastening tool.
|
After pressing a battery release button, the display shows the status of the battery and the fastening tool.
Status
|
Meaning
|
All four LEDs light green.
|
Charge status is 75 % to 100 %.
|
Three LEDs light green.
|
Charge status is 50 % to 75 %.
|
Two LEDs light green.
|
Charge status is 25 % to 50 %.
|
One LED lights green.
|
Charge status is 10 % to 25 %.
|
One LED blinks green.
|
Charge status is below 10 %. The fastening tool is ready for operation.
|
One LED blinks green.
|
The fastening tool is overloaded or overheated and thus not ready for operation.
|