Skip to main content

Swimming pool lane rope anchors

Posted by Jim McConnellabout 1 year ago
Swimming pool lane rope anchors

We are installing a (14) 4" long Bronze tapered hexagon lane rope anchors into an existing gunite wall. Diameter is 1" with staggered hexagons that steps down along the length at 1" intervals. I am planning on using a 1 1/8" carbide hammer drill along with a rebar cutter if needed. It is located in the back wall of a pool gutter which will be at water level but not submerged. I need a recommendation on the strongest anchoring epoxy suitable for wet conditions. Thank you

anchoring epoxy,wet conditions

1 Reply
Posted by Mia Brownellabout 1 year ago
Hilti Verified

Hi Jim,

Hilti does not have any testing for any of our anchors installed into gunite base materials. Gunite is a mixture of sand, cement, and water and therefore, does not align with the base materials that Hilti has testing into: concrete, CMU, and multi-wythe brick. Hilti’s HIT-RE 500 V3 adhesive anchor is suitable for installations into submerged conditions; however, it is only approved for concrete base materials.

Since anchorages into Gunite are outside the scope of Hilti’s testing, the Engineer of Record could consider engineering judgement or on-site testing to account for variability in performance.

If you have any further questions, please reach out to hnatechnicalservices@hilti.com.

Best,

Mia

adhesive anchor