Posted by Matthew Shufflebarger5 months ago
Is HAS-E-55 weldable
Does the HAS-E-55 material meet ASTM F1554 S1 weldability supplement? Thank you.
1 Reply
Posted by Hilti Employee5 months ago
Hi Matthew,
Unfortunately, Hilti does not have testing to confirm whether the HAS-E-55 threaded rods are ASTM F1554: S-1 compliant and weldable. The mill certificate, which can be requested at the time of purchase, should indicate whether it is ASTM F1554 S-1. Typically, engineers avoid welding on or near anchors for the following reasons:
- The mechanical properties of the anchor could be changed resulting in reduced load capacity.
- The corrosion resistance properties of the anchor could be reduced during the welding process.
- The chemical composition of the welding area could be altered and negatively affect performance.
- For adhesive anchors, welding could negatively affect the adhesive bond due to the conduction of heat through the anchoring element.
- Welding does not comply with the approvals of either mechanical or adhesive anchors.
- Welding could remove the length identification mark on the anchor.
- Welding operations on anchors under load is extremely dangerous.
- The combination of different influence factors has not been tested (welding different materials, welding methods, welding quality, etc.).
Ultimately, the engineer on the project will be responsible for deciding if welding is acceptable for their application.
Regards,
Katelyn