Skip to main content

How close to an existing anchor rod can a new epoxy anchor be located if the existing is cut off flush with the concrete, in tact and not being used?

Posted by  Dan6 months ago
How close to an existing anchor rod can a new epoxy anchor be located if the existing is cut off flush with the concrete, in tact and not being used?

Existing cast in place anchor rod must be cut flush with top of footer to allow new column installation. The new column will have a different anchor rod pattern for drilled in place anchors.

anchor,location

1 Reply
Posted by Sinan Beskok6 months ago
Hilti Verified

Hi Dan,

Thank you for reaching out. Conditions where an adhesive anchor is to be installed near an abandoned cast-in-place anchor are ultimately outside of Hilti’s published test data, which lends the decision to engineering judgement by the Engineer of Record on the project. In general, installation wise, this would involve grinding the exposed portion of the old anchor down so that the anchor is receding below the base material's surface; this will allow a fixture to sit flush against the surface in that abandoned anchor's location. Afterwards, the new adhesive anchor would be installed.

It is likely the new anchor's performance will be influenced by the abandoned anchor; refer to the new anchor's supportive testing for spacing considerations to determine the influence that the abandoned anchor may have on the new anchor's capacity. One approach may be to consider the new anchor’s spacing requirements compared to the abandoned anchor spacing requirements then take the more limiting of the two.

When installing the new anchor, care must be taken so that the minimum edge distance for the new anchors (not the abandoned anchor) is not violated. Sometimes when the new anchor is installed there may be a desire to install closer to an edge. It would be critical to ensure the new edge distance is not violating the minimum values, and a new design may need to be performed based on the new geometry.

Ultimately, as the condition is outside of Hilti’s published testing, the approach is at the discretion of the Engineer of Record.

For additional questions, please reach out to hnatechnicalservices@hilti.com

Kind regards,
Sinan

anchor,adhesive,cast-in place,Abandon