Skip to main content

HIT-HY 270 adhesive with threaded rods in the face of fully grouted CMU wall

Posted by DILENDRA MAHARJANover 3 years ago
HIT-HY 270 adhesive with threaded rods in the face of fully grouted CMU wall

As per Anchor Fastening Technical Guide, Edition 22, Page 177, footnote 2, anchors may be installed in any location in the face of the grouted masonry wall including mortar joints.
However, as per Masonry Anchor Design Guide 2023, Page 33, footnote 4, the minimum distance from the center of an anchor to the centerline of a head joint is 2".
Both of these tables apply to HIT-HY 270 installation with threaded rods into solid grouted CMU walls. Please clarify these conflicting requirements. Thank you.

advanced anchor design,Masonry Design,HIT-HY270

3 Replies
Posted by Danielle Filerover 3 years ago
Hilti Verified

Hi Dilendra,

That is correct. The acceptance criteria for testing is different depending on whether it is LRFD or ASD. Under ASD testing, it was tested and deemed acceptable anchoring into the mortar joints for grout-filled CMU applications.

Regards,
Dani


Posted by Danielle Filerover 3 years ago
Hilti Verified

Hi Dilendra,

These two tables are under two different design methods. Traditionally, all masonry anchors fell under allowable stress design (ASD). The code is now transitioning into strength design (LRFD) for masonry, similar to what concrete anchors are tested and designed to now. The Anchor Fastening Technical Guide is based on ASD, where the tables in the new 2023 Masonry Anchor Design Guide pertain to LRFD. There will be some variances between the two and it just depends on what the code requirements are for your specific situation.

Regards,
Dani

LRFD masonry,HIT-HY 270 LRFD,ASD versus LRFD

2 comments on this reply
Posted by DILENDRA MAHARJANover 3 years ago
Thanks, Dani. I understand that Hilti's Masonry Anchor Design Guide 2023 was based on the new AC58 which utilizes LRFD design methods. Is the ASD method even allowed for designing anchors with HIT-HY 270 adhesives? Going forward, does Hilti recommend using ASD or LRFD design methods for masonry anchors?

Posted by DILENDRA MAHARJANover 3 years ago
Thank you Dani for your response. Are you implying that if I design the anchors based on the ASD design method, I can put the anchors in the head joints of the CMU wall? Does Hilti have test data to back this up (tests with the influence of head joints in the wall)?

Posted by Danielle Filerover 3 years ago
Hilti Verified

Hi Dilenadra,

ASD is still an acceptable design method for masonry anchors. Hilti is unable to recommend what design method to use. Typically, the code year used for design and local requirements will dictate what is required. Since buildings are normally a few years behind the code, it will take awhile for masonry ASD to become obsolete.

Regards,
Dani