Skip to main content

Elastomeric Firestopping Sealants and Hydrogen rich environments

Posted by  Michael Bover 4 years ago
Elastomeric Firestopping Sealants and Hydrogen rich environments

Are there any adverse effects of elastomeric firestopping sealants being used in a hydrogen rich environment? Since those sealant are air-tight will they stop that kind of air transfer still in that kind of environment?

Sealant,Hydrogen,elastomeric,effects

2 Replies
Posted by Tyler Thomasover 4 years ago
Hilti Verified

Hello Michael,
My name is Tyler and I work with Fire Protection Engineering department here at Hilti. I am going to check with our Product Care team about this question since we don't have any document stating if there will be any effects or such when the sealant is exposed to hydrogen rich environment.
Tyler


Posted by Tyler Thomasover 4 years ago
Hilti Verified

Hello,
I just heard back from Product Care team. Since Hydrogen is the smallest chemical molecule and gas tightness against H2 is always critical. Even metals are not 100% perfect. However, anything which helps against air will also help against H2. At least CFS-S SIL GG/SL will reduce the gas flow through gaps and cracks, but it won’t be fully tight. And be aware that we have no testing for H2.

We are also curious what is the application since there may be a better solution to use beside elastomeric sealant.


1 comment on this reply
Posted by  Michael Bover 4 years ago
Tyler, Thank you for getting back to us on this item. Our client produces liquid hydrogen and the fire barrier in question is within one of our buildings between two equipment rooms. This wall obviously requires firestopping, but they wanted to know more about how the elastomerics would perform again H2 infiltration. I believe your answer above will suffice since it appears that since it is an air barrier it will perform as expected with very little infiltration.