Added to cart
Added to cart
Go to shopping cart

Compliance Resources

Hilti ON!Track

Documentation Management Tool

Customers impacted by OSHA 29 CFR 1926.1153 (Silica Dust Regulation) will need to have documentation readily available for specific assets and applications. ON!Track can manage various OSHA required documentation and allow it to be accessible, not just in an office but on a jobsite as well. Click here to speak with one of our specialists to learn how ON!Track can help you with the below documentation.

  • Objective Data documentation
  • Operating instructions
  • Any company specific requirements

Manage Employee Certifications And Trainings

Navigating the new OSHA silica dust regulation (1926.1153) goes beyond understanding the rules and having the proper equipment. The new standard states that compliance with the Hazard Communication Standard (29 CFR 1910.1200), includes training workers on the silica hazard, the health effects of exposure, protective measures, the identity of the competent person, and the medical surveillance program. How can a company stay on top of tracking these trainings and others? The answer is Hilti ON!Track, our comprehensive asset management solution.

ON!Track is a secure web based application that is accessible from any device with an internet connection. ON!Track allows contractors to manage several trainings and certificates for each employee, receive alerts as renewals are needed, and easily generate reports. Because ON!Track’s primary focus is managing assets and equipment, the system will also alert you if you try to transfer a piece of equipment to an individual who does not possess the proper training or licensing to operate it.

Share

Log in to proceed
Need help? Contact us
Register now
CONTACT US
CONTACT US