Using ON!Track to track documents

Documentation management tool

Customers impacted by OSHA 29 CFR 1926.1153 (Silica Dust Regulation) need to have documentation readily available for specific assets and applications. ON!Track can manage various OSHA required documentation and allow it to be accessible in the office and on the jobsite.

Request a consultation and learn how ON!Track can help you with the following types of documentation:

  • Objective Data documentation
  • Operating instructions
  • Any company specific requirements

Manage Employee Certifications And Trainings

Navigating the OSHA silica dust regulation (1926.1153) goes beyond understanding the rules and having the proper equipment. This standard states that compliance with the Hazard Communication Standard (29 CFR 1910.1200), includes training workers on the silica hazard, the health effects of exposure, protective measures, the identity of the competent person, and the medical surveillance program. How can a company stay on top of tracking these trainings and others? The answer is Hilti ON!Track, our comprehensive asset management solution.

ON!Track is a secure web based application that is accessible from any device with an internet connection. ON!Track allows contractors to manage several trainings and certificates for each employee, receive alerts as renewals are needed, and easily generate reports. Because ON!Track’s primary focus is managing assets and equipment, the system will also alert you if you try to transfer a piece of equipment to an individual who does not possess the proper training or licensing to operate it.

Share