Quantity Updated
Please note, the order volume has been updated. This is due to package and minimum order quantities.
Please note, the order volume has been updated to. This is due to package and minimum order quantities.
Chemical anchoring is a method of fastening in which a metal insert is bonded to concrete. At Hilti we have two types of chemical anchors, Resin Epoxy and Hybrid Adhesives, that are designed to give the installer greater flexibility depending on the application.
Chemical anchors can be used in a variety of different applications but some of the most common ones are:
Share
To see account specific prices and content, please choose appropriate account.