The Project
South Beach is a mixed-use development strategically located on the border of Singapore’s central business district, according to the South Beach Consortium. The development seamlessly blends four historic buildings on site with two new towers to feature offices, luxury residences, a designer hotel, retail spaces and an exclusive membership club.
One of South Beach’s unique eco-friendly features is its microclimatic canopy that extends throughout the development. The canopy is engineered to harvest rainwater and is fitted with photovoltaic cells to convert solar energy into electricity. Winner of two Green Mark Platinum Awards, the development’s green efforts are further supported by its good orientation, high-performance glass façade and extensive sky gardens which help to absorb heat and maintain a high level of thermal comfort throughout the day. In addition, energy and water efficient fittings and certified green label building materials all contribute to South Beach’s commitment to being one of Singapore’s most environmentally conscious developments.