Quantity Updated
Please note, the order volume has been updated. This is due to package and minimum order quantities.
Please note, the order volume has been updated to. This is due to package and minimum order quantities.
Please note, the order volume has been updated. This is due to package and minimum order quantities.
Please note, the order volume has been updated to. This is due to package and minimum order quantities.
Hilti’s mechanical anchor portfolio offers something for every designer from low capacity removable screw and sleeve anchors to medium-duty wedge anchors to high capacity expansion and undercut anchors.
Commonly known as concrete anchors, though many are also suited for installation in masonry, mechanical anchors do not have the installation and in-use temperature restrictions of their adhesive anchor counterparts. Additionally, mechanical anchors can be loaded immediately after installation whereas an adhesive anchor must be fully cured before loading. This flexibility offers design freedom to the specifier and added productivity to the contractor.
While adhesive anchors transfer loads to the base material via the bond of the adhesive element, post-installed mechanical anchors transfer the load to the base material through bearing, friction or keying.
Wedge anchors transfer loads by friction, and to some extent bearing / keying. Examples of these anchors are the Kwik Bolt TZ, Kwik Bolt 3 and the HSL-3. Screw anchors are inserted into a drilled hole that is typically smaller in diameter than the actual anchor. The loads are then transferred to the base material by keying. An example of a screw anchor is the Kwik HUS-EZ. Undercut anchors derive their holding strength from the mechanical bearing interlock provided from the undercutting of the concrete at or near the bottom of the hole achieved either by a special tool or by the anchor itself during installation. An example of an undercut anchor is the HDA.
Understanding how different mechanical anchors transfer loads to which base materials is key to understanding which anchors provide the appropriate holding values for your loading situation and knowing which one to select for your next project design.
Our executive will call you back shortly
An e-mail has been sent to our Customer Service team for follow-up. You will receive a copy of your request for your records.
To see account specific prices and content, please choose appropriate account.
Hilti = registered trademark of Hilti Corporation, 9494 Schaan, Liechtenstein © 2009-2016, Right of technical and programme changes reserved, S.E. & O
Our executive will call you back shortly
An e-mail has been sent to our Customer Service team for follow-up. You will receive a copy of your request for your records.