Added to cart
Added to cart
Go to shopping cart

Put away your torque wrench

Achieve ICC-ESR and ETA compliance for wedge anchor installation into concrete with the new Adaptive Torque System

Adaptive Torque System

To correctly install an anchor, your choices are between a slow torque wrench, cumbersome torque bars, or a powered impact wrench which lets productivity soar while safety and reliability slump.

Now, with Hilti's Adaptive Torque (AT) system, you don’t have to compromise.*

*Currently designed for select sizes of Hilti KB-TZ and KB3 anchors only. Contact Hilti for details.

The AT system is made up of four components:

  • The cordless impact wrench SIW 6AT-A22: it looks and works like the Hilti SIW 22-A cordless impact wrench but with intelligent electronics, a more robust anvil, and a sleeker front part which can reach into tighter spaces.
  • SI-AT-A22 module: a small, very light interface which slots in between the impact wrench and battery and processes live data from the SIW 6AT-A22 to recognize when an anchor has been correctly installed.
  • Documentation software so that the SI-AT-A22’s job history can be transferred to a PC and used to create a detailed installation report.
  • Hilti KB-TZ and KB 3 expansion anchors for cracked and un-cracked concrete.

AT-ready tools are equipped with the sensors and on-board intelligence to confirm if an anchor has been set according to ICC-ESR approvals. The operator simply inputs which anchor is being used – as easy as scanning the box with the SI-AT-A22’s integrated barcode reader – and the tool does the rest. Afterwards, the tool can be connected to a computer to instantly generate an installation report, offering inspectors and specifiers a higher confidence that the work has been carried out exactly as specified.

Simple, Fast, Effective

Select your anchor

Use the SI-AT-A22 module’s built-in scanner to read the barcode on your box of anchors. The SIW 6AT-A22 impact wrench then adjusts the torque setting to meet certification report requirements. Tap the lock button to confirm your selection, and the impact wrench is ready to use.

SIW 6AT adaptive torque system application

Pull the trigger

With the SIW 6AT-A22, all you need to do is pull the trigger and let the tool work. As soon as the SI-AT module lights up green, you know the anchor has been torqued to the right level to comply with ETA and ICC-ESR approvals.

SIW 6 AT and adaptive torque system

Done, done right.

Giving you more confidence that the anchor has been correctly installed, sensors in the SIW 6AT-A22 recognize if an anchor has been loosened and, on retightening, will restore the correct torque. And with the AT System you can adjust and retorque up to three times.

Adaptive Torque System in Action

alt text

Easily generate your installation report

Please enter alternative text here (optional)

Full accountability has never been easier. Simply connect the SI-AT-A22 module to a computer using a standard printer USB cable and the AT Documentation Software then downloads performance data stored by the SI-AT-A22, which can be used to produce an installation report.

The report lists all products used, the method of selection (scan or manual) and completion time and date.  

From a specifier’s perspective, this report proves that the anchors have been torqued correctly to certification report requirements. From an installer’s point of view, it can help you breeze through site inspections.

Changes encouraged

Please enter alternative text here (optional)


The SIW 6AT-A22 is intelligent enough to detect an anchor which has been tightened and then loosened again, a function which is useful for straightening or aligning neighboring fixtures, such as railings and windows.

During this process the SI-AT-A22 module will use an algorithm, developed from over 10,000 tests, to retighten the anchor ensuring no improper torqueing occurs. Once the tool stops, the SI-AT-A22 provides a visual indication to the operator that the anchor has been retightened by flashing a yellow light, displaying a notification on the display and a sound. The anchor must then be checked with a calibrated torque wrench to ensure proper torque has once again been achieved.

SafeSet Technology

The anchor setting trifecta: SafeSet

Please enter alternative text here (optional)

Safety. Productivity. Approval. SafeSet is Hilti’s proven methodology for consistently high-quality anchor installation at lightning speed.

The SIW 6AT-A22, along with the SI-AT-A22 module, fulfills all SafeSet criteria because they save time and reduce costs while also reducing the potential for installation error. 

SafeSet technology provides new ways for engineers and contractors to minimize installation errors.

Learn how 

PROFIS Anchor Design Software
Profis Anchor Design Software

Hilti PROFIS Anchor technology allows designers and specifiers to quickly, easily evaluate Hilti anchor products and systems—and then choose the best solution for any conditions.

Learn more about PROFIS Anchor
Adaptive Torque Documentation Software
Adaptive Torque Documentation Software

Installation Report Software for the SI-AT-A22 Module.

Learn more
specifications and cad details
Specifications, General Notes and CAD Details

Incorporate Hilti anchor products into your designs.

Learn more
ask Hilti
Ask Hilti

Our online community offers expert advice from top engineering professionals.

Visit Ask Hilti

Share

Log in to proceed
Need help? Contact us
Register now
CONTACT US
CONTACT US